Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How is the Auto restart function activated on ATV12?
Issue:
ATV12 auto restart function activation.

Product Line:
ATV12, Altivar 12

Environment:
All

Cause:
NA

Resolution:
NOTE: This function allows an automatic restart of the drive controller if the cause of the fault has disappeared and a run command is maintained. It also allows the drive to restart after a power loss. Please make sure that this condition is safe for your application. Auto restart does not restart the drive for all of the fault conditions. With certain faults the drive controller must be reset by cycling power.
Please refer to the documentation associated with the product for further information, cautions or warnings that may apply to this issue.



Go to ConF, Full, I-O-, tCt and set 2 wire type to level control (LEL).
Go to ConF, Full, Flt, Atr, again Atr and set auto fault reset to yes (Yes).

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings