Issue:
How do I prevent an ATV630 series process drive from running in reverse?
Product Line:
ATV630 series
Environment:
All models, All serial numbers.
Cause:
Information difficult to find in user manual.
Resolution:
Under menu 5, Complete settings, navigate to sub menu 5.5, Command and Reference. Locate the Reverse Disable parameter and set it to Yes.
How do I prevent an ATV630 series process drive from running in reverse?
Product Line:
ATV630 series
Environment:
All models, All serial numbers.
Cause:
Information difficult to find in user manual.
Resolution:
Under menu 5, Complete settings, navigate to sub menu 5.5, Command and Reference. Locate the Reverse Disable parameter and set it to Yes.
Released for: Schneider Electric Nigeria