Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert - ION_Data Archive Task fails due to insufficient permissions for IONMaintenance.

Issue
The Power Monitoring Expert installer will set up Windows Scheduled Tasks for a number of database-related tasks. One of these tasks is to run database archives on a scheduled basis. By default, these Windows tasks are set up to use the IONMaintenance Windows account and is installed in a disabled state. If the task is enabled, it fails.

Product Line
Power Monitoring Expert 8.0

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024


Environment
Database Archiving

Windows Tasks Scheduler

Cause
That task fails because the IONMaintenance Windows account does not have the required permissions to create an archived database.

Resolution
If this task is to be used, it is necessary to change the Windows account that the Windows task uses to an account that is a member of the sysadmin role in SQL Server. This is because the archive task will create a new database, and sysadmin level privileges are required to do this.

Note: As of PME 8.2, the Windows database tasks are not set up in distributed systems that use a separate database server.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings