Issue:
Do the XVGU and HMIZRA1 USB accessories need powered USB hubs to function with the HMIG3U?
Product Line:
Magelis HMIG3U
Resolution:
The HMIG3U does not need a powered USB hub to power the XVGU and HMIZRA1. Each of the USB ports of the HMIG3U can supply upto 500ma of current. The two devices require 400ma each
Do the XVGU and HMIZRA1 USB accessories need powered USB hubs to function with the HMIG3U?
Product Line:
Magelis HMIG3U
Resolution:
The HMIG3U does not need a powered USB hub to power the XVGU and HMIZRA1. Each of the USB ports of the HMIG3U can supply upto 500ma of current. The two devices require 400ma each
Released for: Schneider Electric Nigeria