Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use a monitor with 4K resolution with Unity?
The display properties of the 4K or even simply a high resolution monitor can make using Unity somewhat of a challenge. Although you'll be unable to use the full resolution of this type of monitor you can make a few simple adjustments which will allow you to use Unity.

Please see attached.


Schneider Electric Nigeria

Attachment(s)
res_scr.docx [304.26 KB]