Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV212 preset speed function override PID control?
Issue:
Overriding PID control with ATV212 preset speed function.

Product Line:
Altivar 212 ATV212

Environment:
All models

Cause:
Activation of preset speed needs to override PID control

Resolution:
The preset speed activation does not override PID control.  When activating the logic input for a preset speed, also activate a separate logic input that is assigned to 14 (PID disable) to deactivate PID control.  This way, the preset takes control.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings