Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What parameter do you change to set up the ATV320 drive to run on a fan or pump application?
Issue:
Set up the ATV320 drive to run on a fan or pump application.

Product Line:
Altivar ATV320

Environment:
All

Cause:
Want to set up the ATV320 for fan and pump applications.

Resolution:
The ATV320 works well on variable torque and constant torque applications.  The default is for common constant torque loads.  A centrifugal pump and fan are variable torque loads.  Set the Motor control type to V/F Quadratic.

Go to Conf -> FULL
Menu drC
Parameter Ctt, set to [V/F Quad.]
(UFq): Variable torque. For pump and fan applications.

Schneider Electric Nigeria

Attachment(s)
ATV320_programming_manual_EN_NVE41295_01.pdf [2.05 MB]