Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would prevent a Control Expert (formerly Unity Pro) Quantum PLC from performing CCOTF successfully?
- In order for CCOTF to perform successfully you need to enable the feature in the PLC configuration prior to initial download.
- The CRP and CRA interfaces must also be using a  firmware version capable of performing CCOTF. You can check %SW98 and %SW99 to verify if these interfaces are CCOTF compliant.

Schneider Electric Nigeria

Attachment(s)
CCOTF selection.docx [188.52 KB]