Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Structured Text user function block to return the Day of the Week

DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.



ClearSCADA allows the user to create its own Structured Text library, where several user function blocks can be stored.
A function that is periodically requested by users is one that returns the day of the week from a DATE_AND_TIME input variable. The code below returns the day of the week as a number (0 = Sunday to 6 = Saturday):

FUNCTION_BLOCK DayOfTheWeek

VAR_INPUT
InDate : DATE_AND_TIME;
END_VAR

VAR_OUTPUT
DayOfWeek : INT;
END_VAR

VAR
Year : INT;
cYear : INT;
Month : INT;
Day : INT;

CP : INT;
YP : INT;
MP : INT;

LeapYear : BOOL := FALSE;
Valid :BOOL;
END_VAR

Year := EXTRACT_DT_YEAR(InDate);
cYear := STRING_TO_INT(RIGHT(INT_TO_STRING(Year),2));
Month := EXTRACT_DT_MONTH(InDate);
Day := EXTRACT_DT_DAY(InDate);

Valid := TRUE;
CASE Year OF
1752..1799 : CP := 4;
1800..1899 : CP := 2;
1900..1999 : CP := 0;
2000..2099 : CP := 6;
ELSE  Valid := FALSE;
END_CASE;

YP := cYear / 4;

IF (MOD(cYear,400) = 0) THEN
LeapYear := TRUE;
ELSIF (MOD(cYear,100) = 0) THEN
LeapYear := FALSE;
ELSIF (MOD(cYear,4) = 0) THEN
LeapYear := TRUE;
ELSE
LeapYear := FALSE;
END_IF;

CASE Month OF
1 :
IF LeapYear THEN
MP := 6;
ELSE
MP := 0;
END_IF;
2 :
IF LeapYear THEN
MP := 2;
ELSE
MP := 3;
END_IF;
3 : MP := 3;
4 : MP := 6;
5 : MP := 1;
6 : MP := 4;
7 : MP := 6;
8 : MP := 2;
9 : MP := 5;
10 : MP := 0;
11 : MP := 3;
12 : MP := 5;
END_CASE;

IF Valid THEN
DayOfWeek := MOD(CP + cYear + YP + MP + Day, 7 );
ELSE
DayOfWeek := -1;
END_IF;

END_FUNCTION_BLOCK


Once added to a library, this function can be called from both ST or FBD logic program.
Below a picture of the function being called from an FBD program:
FBD

Below a picture of the function being called from an ST program:
Structured Text

Note: Don't forget to add the library that contains the function block you are going to use to your logic program before calling the function. For more information on how to do that, please search the manual for "ST and Function Block Libraries".

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: