Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I perform a hypot test on an Altivar drive, or a circuit with an Altivar drive installed?
Issue:
Hypot test on an Altivar drive.

Product line:
All Altivar products.

Environment:
All models, All serial numbers.

Cause:
Information unavailable in current literature.

Resolution:
It is not recommended to perform a hipot test on an altivar drive or with an altivar drive in circuit, where the test is being performed.  The drives are tested 100% in production.  If the high potential test is not performed properly, or if the voltage and/or dwell time are incorrect, the drive can be damaged.  Damage to the drive caused by a high potential test is considered abuse and will not be covered under warranty.