Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set up fault reset over the network with the ATV630 drives embedded Ethernet in I/O profile mode?
Issue:
ATV630 drives embedded Ethernet in I/O profile mode set up fault reset over network.

Product Line:
ATV630 or ATV930 in I/O Profile mode only

Environment:
All

Cause:
Wants to reset the faults over Ethernet using Bit 1 of the command word CMD.

Resolution:
With Profile set to I/O the assignment for fault reset will be C501 as fault reset being Bit 1 of the CMD with embedded Ethernet and I/O profile.
C501 means Bit 1 of the CMD 8501 will allow the faults to be reset over the embedded Ethernet network.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings