Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement power board part numbers for ATV71 drives?
Issue:
ATV71 replacement part number for power bard.

Product Line:
Altivar 71

Environment:
It is required to check the Serial number of the drive before ordering the Power Board.
If the 8th digit in the serial number is 2, the drive was built using Fuji IGBT's instead of the standard Mitsubishi IGBT's.   A drive with Fuji IGBT's requires a modified version of the Power board (VX5A1HC1113F).   IGBT, and gate driver board parts also will have an F at the end.

Cause:
Replacement parts.

Resolution:
ATV71 power board
AVAIL. = Available as of this date
*FS= Parts are only available from Field Services and require FS installation.
NR = Not replaceable
Obs = Obsolete no longer available
The drive MAY be repairable even if parts are no longer available for sale.  Contact Schneider Electric Industrial Repair Service (SEIRS) at 800-950-9550
Contact your local Schneider Electric distributor for a replacement drive. (search here)
New!  Try our Drive and SoftStart selection tool for self selection (open style devices)
Technical Support for AC drives and soft starters: 888-SQUARED (888-778-2733) select option 1 for Technical Support and then option 4 for AC Drives and Softstarts.
Technical Support is available from 8am EST to 8pm EST M-F and 24 hours a day for EMERGENCIES.