Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV930 drive is getting an Embedded Ethernet Comms failure when connected to the Ethernet IP network.
Issue:
What is an Embedded Ethernet Error on an ATV900 series drive?  Customer is using Ethernet IP communication.

Product Line:
Altivar 900
ATV930
ATV960
ATV980

Environment:
Embedded Ethernet

Cause:
The RSTP function is enabled by default and it not accessible from the HMI

Resolution:
Look at the attachment.

Schneider Electric Nigeria

Attachment(s)
Capture.PNG.png [37.46 KB]