Issue:
What is the size of the PM8000's FTP site?
Product Line:
PM8000 series meters
Environment:
PM8000 FTP site memory
Cause
Unable to find the size of the FTP site memory
Resolution:
The FTP site for a PM8000 meter is approximately 350 MB in size. This includes the directories for webpages, Comtrade, and IEC61850 files. The default webpages weigh in at around 5 MB. These can be removed to free up more FTP space, if required for custom web pages.
What is the size of the PM8000's FTP site?
Product Line:
PM8000 series meters
Environment:
PM8000 FTP site memory
Cause
Unable to find the size of the FTP site memory
Resolution:
The FTP site for a PM8000 meter is approximately 350 MB in size. This includes the directories for webpages, Comtrade, and IEC61850 files. The default webpages weigh in at around 5 MB. These can be removed to free up more FTP space, if required for custom web pages.
Released for: Schneider Electric Nigeria