Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the current consumption (burden) of IRIG-B port in ION8650 meter?
Product Line
ION8650

Environment
Hardware

Resolution
The input impedance on the IRIG-B port (red to black) is 450 kΩ. So for a 5 V input voltage, the current draw would be around 0.01 mA.