Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reset the Digital Input count on a CM2000

Issue
Customer would like to reset the digital input status counter on the CM2000.

Product Line
CM2000 series

Environment
Modbus Register writes

Cause
The CM2000 does not have a digital input status counter reset command.

Resolution
Using Modbus Tester, write a value of zero (0) to the desired registers. Below is an excerpt of the CM2000 Modbus Register list that details the Digital Input's registers.

RegistersRange
Input 1 Count2404 - 24050 to 99,999,999
Input 2 Count2409 - 24100 to 99,999,999
Input 3 Count2414 - 24150 to 99,999,999
Input 4 Count2419 - 24200 to 99,999,999
Input 5 Count2424 - 24250 to 99,999,999
Input 6 Count2429 - 24300 to 99,999,999
Input 7 Count2434 - 24350 to 99,999,999
Input 8 Count2439 - 24400 to 99,999,999


In the following example, a CM2350's Input 1 Count is going to be reset. The necessary parameters are as follows:

  • Gateway IP Address: 10.167.244.21
  • CM2350 Device ID: 9
  • Starting Register: 2404

Once all the parameters have been specified, press Write to reset the value.

IMG1

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: