Issue
PowerLogic devices with digital I/O alarms do not have the ability to add delays.
 
Product Line
EcoStruxure™ Power Monitoring Expert 8.X
 
Cause
PowerLogic devices such as CM4000 and PM800 devices have the ability to alarm on digital input status changes. Unfortunately there is no way to program a delay into the logic.
Resolution
With PME 8 and alarm configuration we now have the ability to add delays to digital alarms. Adding a delay would make the alarms more consistent with other alarms that have delays built into them.
 
PowerLogic devices with digital I/O alarms do not have the ability to add delays.
Product Line
EcoStruxure™ Power Monitoring Expert 8.X
Cause
PowerLogic devices such as CM4000 and PM800 devices have the ability to alarm on digital input status changes. Unfortunately there is no way to program a delay into the logic.
Resolution
With PME 8 and alarm configuration we now have the ability to add delays to digital alarms. Adding a delay would make the alarms more consistent with other alarms that have delays built into them.
Released for: Schneider Electric Nigeria