Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the purpose of firmware upgrade in energy meter ?

Issue
What is the purpose of a firmware upgrade in an energy meter?


Product line
PowerLogic™ Energy Meters (including PM series such as PM2225)

Environment
Energy metering systems where performance optimization, feature enhancements, or compliance updates are required

Resolution

There are several reasons to upgrade your meter’s firmware:

  • Improve meter performance (e.g. optimize processing speed)
  • Enhance existing features and functions
  • Add new functionality to the meter
  • Ensure compliance with new or updated industry standards

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings