Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does PME support the UDP protocol?
Issue
A customer would like to know if PME supports the UDP protocol.

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x

Environment
Supported communications protocols

Cause
The User Database Protocol provides no guarantees for message delivery and the UDP layer retains no state of UDP messages once sent.
For this reason, UDP is referred to as an 'unreliable protocol' and is not suitable for real time data or historical data logs.

Resolution
UDP is not supported by PME.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: