Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
U.motion KNX Server Plus, Touch. Can't you finish the booting and start the system?
This document cover
MTN6260-0410, U.motion KNX Server Plus, Touch 10
MTN6260-0415, U.motion KNX Server Plus, Touch 15

Questions again
Do you face a problem with booting process of those devices?
Can't you finish the booting and start the system?
Does the display show this message: Disk boot failure, insert system disk and press enter?


Causes and fixies
The file system on flash card is probably corrupted. To fix the problem is to insert the flash card with correct file system. This new CF card should be sent to you. Because the file system is linked with particular serial number you should provide the serial number of the device. When you/customer will receive the CF card the device should be uncovered and the card changed in the slot.

Please provide a text or photo of the message. Some description if necessary.
Precise type number, serial number of the device. It is labeled on back side of the device.
The address where the CF card with a new system should be delivered.

Schneider Electric Nigeria

Attachment(s)
umotion_touch.png [490.88 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: