Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Explain the digital input characteristics of PM3255?

Issue

Explain the digital input characteristics of the PM3255 meter.

Product Line

PowerLogic™ PM3255 Series Meter.

Environment

Energy monitoring systems requiring digital input functionality for control, metering, and event-based operations.

Resolution

The PM3255 meter supports 2 digital inputs, designated as DI1 and DI2, with four configurable operating modes:


Digital Input Operating Modes

  1. Normal Input Status

    • Used for simple ON/OFF digital inputs.
    • Can monitor OF (Open Fault) or SD (Switch Disconnected) signals from circuit breakers.
  2. Multi-Tariff Control

    • Tariff control can be managed via communications, internal clock, or 1–2 tariff inputs.
    • Applying specific ON/OFF signal combinations to the inputs allows the meter to register energy under different tariff registers.
  3. Input Metering

    • Used for WAGES (Water, Air, Gas, Electricity, Steam) applications.
    • Configure pulse frequency (pulse/unit) to count pulses and calculate units.
    • Note: Pulse width or stop duration less than 10 ms is invalid for counting.
  4. Energy Reset

    • Resets partial energy, energy by tariff, and energy by phase.
    • Activated by an ON signal lasting more than 10 ms.