Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use network braking unit for Altivar ATV930 ?

Yes, there is new range of network braking units ATVRU75N4 (7.5kW unit) and ATVRD15N4 (15kW unit).
It is possible to combine up to 3 units in parallel. ATVR is compatible with Altivars: ATV320, ATV340 and ATV900.
Manual (NVE88423) and sizing tool (NVE94856) can be downloaded from schneider web.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings