{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Does the W870-8135 NetShelter key work on the combination handle AR8132A?
Issue: 
A customer claims that their new AR8132A door handles can be opened with the standard NetShelter 333 key: W870-8135. 

Product Line: 
NetShelter SX, AR8132A

Environment: 
All models, all serial numbers. 

Cause: 
The AR8132A uses a different key, but the standard 333 key will also open the lock. 

Resolution: 
The AR8132A will accept any key similar when the combination is set to the factory default of 000. 
Once a new combination is set, only the key included with the AR8132A will open the lock. 

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top