Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will a surge protector protect against temporary over voltages?
Surge protectors are not intended to safeguard against over voltages below the surge protector's maximum continuous operating voltage (MCOV). For a 120V-based surge protector, the MCOV is 150V line to neutral and line to ground. For 480/277Y, the MCOV is 320V line to neutral and line to ground. For 600/347Y, the MCOV is 420V line to neutral and line to ground.

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: