Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Wrong Power Budget for BME NOS 0300 on Unity Pro V13 and below (V12, V11.1)
Unity Pro calculates automatically Power Budget for controller configuration, based on maximum Power consumption of modules configured. It generates a warning in case total Power budget is superior to the Power supplied.

The BME NOS 0300 Power consumption budget taken into account by Unity Pro versions V13 and below (V12, V11.1) is not correct.

Unity Pro V13 (and below) states:
3,3V      0,5A                   1,8W

While the correct values are :
3.3V      0,02A                  0.066W
24V        0,2A                   4.8W
Those values will be updated in next Unity Pro release (V13.1)