Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you order the series E bypass circuit on the S-Flex enclosed drives?
Issue:
Trying to order the series E bypass circuit on the S-Flex enclosed drives.

Product Line:
S-flex enclosed drives with bypass

Environment:
All

Cause:
The manual shows series D with AFC off bypass and Series E with AFC/Bypass with Hand off auto

Resolution:
The series E hand off auto with AFC/Bypass is the only option now.  The D series was a carry over from the previous S-flex Series.
So if you place a quote to order with bypass it will come with the E series AFC/bypass and hand off auto.

Schneider Electric Nigeria

Attachment(s)
Instructiosn Bull_30072-451-83_04_Final.pdf [3.69 MB]