Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the recommended lug kit for a Frame Size 6 Process Drive?

Article available in these languages: Spanish

Issue:
Frame Size 6 Process Drive Lug kit part number

Product Line:
Altivar Process Drives (ATV6xx, ATV9xx) Frame Size 6

Environment:
All

Cause:
NA

Resolution:
This applies only to frame size 6, which includes the following drive part numbers:
ATV630D55M3ATV930D55M3C
ATV630D75M3ATV930D75M3C
ATV630C11N4ATV930C11N4C
ATV630C13N4ATV930C13N4C
ATV930C16N4ATV930C16N4C

The part number for the Lug Kit is DZ2FH6. This kit has quantity of 6 lugs. Individual lugs can be ordered with part number DZ2FH1.
This document provides further detail an installation instructions: https://www.se.com/ww/en/download/document/NHA95647/

Schneider Electric Nigeria

Attachment(s)
ATV_Process_size6_IS_LUG_kit_NHA95647_00.pdf [1.28 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings