How can we help you today?

PlantStruxure PES[4.2 SP3] System Server cannot start

Problem: System Server cannot start with error "The program can't start because D3DCOMPILER_47.dll is missing from your computer. Try reinstalling the program to fix this problem."

IMG_1

Solution: This issue may occur because Windows Update was recently applied and a restart of the OS is pending. Restart the Operating System and then run System Server again. This should resolve the problem.
If the problem persists then contact technical support via psxpes.support@schneider-electric.com.