Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you set up preset speeds on the ATV630 and ATV930 drives?
Issue:
Set up preset speeds on the ATV630 and ATV930 drives.

Product Line:
Altivar Process ATV600 ATV900

Environment:
All

Cause:
Setting up preset Speeds

Resolution:
Under the Main menu, go to Complete Settings > Generic Functions > Preset Speeds > 2 Preset Freq = DIx, then Preset Speed 2 = desired frequency.
Additional preset speeds can be set with > 4 Preset Freq = DIy, then set Preset Speed 3 and 4 as desired.  A total of 16 preset speeds are available. The manual contains a truth table that explains which inputs need to be On/Off for multiple Preset Speeds to work.  See the attached excerpt from the manual.

https://www.se.com/us/en/download/document/EAV64318/

Schneider Electric Nigeria

Attachment(s)
ATV600 Preset Speeds bit table.JPG.jpg [85 KB]