Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where is the family.DSC file located for installation of the TCPOpen Library for Control Expert (formerly Unity Pro)?

Issue:

Where is the family.DSC file located for installation of the TCPOpen Library for Control Expert (formerly Unity Pro)?

Product Line:

Control Expert,  Unity Pro, TCPOpen Library

Resolution:

TCPOpen Library install for Control Expert (Unity Pro).
Run setup.exe from the TCPOpen installation CD.

The path to the family.dsc file requested by the <Install Family> button depends on the Windows OS:

Windows XP

C:\Documents and Settings\All Users\ApplicationData\Schneider Electric\Control Expert 14.0\custom Libset\V7.0\TCPOPEN\FFBinstall\Advanced


Windows 7:

C:\Program Data\Schneider Electric\Unity Pro\Custom Libset\V7.0\TCPOpenInstall\FFBinstall\Advanced


Note:
During the install you may run into a The LibPath key was not found in registry error.

To correct this, Run Updateforcompanions.bat from the folder on the Unity PRo Installation CD.
"UpdateForCompanions" followed by the letter corresponding to the installed Unity Pro package: "S", "M", "L", "XL"
- For example, D:\updateforcompanions XL.bat

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)