Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is is possible to invert analog input on Altivar 212? When 10V is present I want zero speed and if 0V then to run at HSP speed.

This is possible using the scaling for VIA input by means of parameters F201-F204.
With setting:
F201=100%
F202=0Hz
F203=0%
F204=50Hz
you get 0Hz reference at 100% signal on VIA and 50Hz reference at 0% signal on VIA.
Bear in mind the safety.
If 10V signal is lost, Altivar 212 will not be able to recognize the problem. Instead, Altivar 212 will see 0V on its analog input and accelerate motor to HSP.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings