Issue: It is not possible to perform the Active Trip Curve Test for Earth Leakage protection using Ecoreach.
Cause: The Dual Setting is not enabled from the Micrologic X HMI and the Set B is set to active. To perform the Active Trip Curve Test for Earth Leakage protection using Ecoreach switch set A to be active using Ecoreach.
Cause: The Dual Setting is not enabled from the Micrologic X HMI and the Set B is set to active. To perform the Active Trip Curve Test for Earth Leakage protection using Ecoreach switch set A to be active using Ecoreach.
Released for: Schneider Electric Nigeria