Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Clarify bar code use on primary packaging
Depending on the number of products packaged in the primary packaging, the barcode could be EAN13 (1 single product) or EAN14 (several products)
In EAN14 barcode:
  • The first digit is the "Logistic Variant", also named as "Packaging indicator".
  • The next 12 digits are representing the product number. General this the EAN-13 number without the check digit.
  • The last digit is the check digit. ActiveBarcode calculates this digit automatically
More information on barcode: https://www.activebarcode.com/codes/ean14.html
Last digit calculation: https://www.gs1.org/services/check-digit-calculator