Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to pull the program back out of a SCADAPack 334E and open it with Workbench?
Yes you can Upload a Project from SCADAPack E to the workbench Program as instructed below

Uploading a Project from the Target to the Workbench

The SCADAPack Workbench allows a project's source to be retrieved from the IEC 61131-3 target if it was originally build with the Embedded Zip Source resource property.

Please find attached more details from CAM5 Help


Schneider Electric Nigeria

Attachment(s)
Downloading a Workbench Project to the Target.pdf [156.48 KB]