Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wiring diagram of serial cable to connect Vison RTU with RJ-45 based RS-232 port of ScadaPack 350 RTU ?

RJ-45 to SCADAPack Vision

This cable is used to connect from the COM3 (RJ-45-based RS-232) port on the RTU to a DE-9S connector on a SCADAPack Vision. A 1.5 m (5 ft.) long cable is available from Schneider Electric using part number TBUM297237.

RJ-45 to SCADAPack Vision cable Description

RJ-45
8 Pins

SCADAPack E Function

SCADAPack Vision Function

DE-9S

Shield connects to shell

6

TxD

RxD

2

5

RxD

TxD

3

4

GND

GND

5

3

DTR / Test 2

ON switch

1

2

DCD / Test 1

ON switch

4

1

+5 Vdc Out

+5 Vdc In

9

7 and 8 are not connected at this end.

Wires not connected at this end.