Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do Schneider products support the Large Forward Open in CIP communications
Issue
Ethernet/IP supported Frame format

Product Line
M580, M340, Quantum.

Environment
Unity Pro

Resolution
Schneider Products use Large Forward Open for Class 1 connections but only for CRAs. This type of connection is not available to other devices.