Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can One Line's be animated in Power Monitoring Expert?
Issue
Need to animate one-line diagram

Product Line
EcoStruxure Power Monitoring Expert 8.2

Environment
Power Monitoring Software

Cause
Previous versions of PME did not have this capability.

Resolution
The new MultiState Display Module in Power Monitoring Expert 8.2 will allow for this.
For instructions on how to use this module please download the attachment at the bottom of this FAQ. This will provide a detailed operation and use of the new MultiState Display Module.

Schneider Electric Nigeria

Attachment(s)
7EN02-0290-10_ION_Reference.pdf [9.47 MB]