How can we help you today?

How many alarms can display on alarm viewer in M580 web server?

the alarm viewer is the same as the diagnostic viewer in Unity, the message number is depending on the diagnostic buffer in CPU (4Kb-8Kb according to different CPU types).
When the diagnostic buffer is full, the new alarm will not be written. %S77 indicating if the buffer is full or not.