How can we help you today?

Why M580 's application backup function is not available after build change in using some application?

For some specific application, M580 need to take a long time to perform application backup after online build change under cyclic mode for MAST task, during this time, the backup function is not available.  So the backup function is fine it is just a timing problem.
This feature will be enhanced since on M580 SV2.5.
The workaround for current M580 version is to use the periodic mode for MAST task.