Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Configuring MBP_MSTR Function to Explicit Read Quantum PLC via Native Modbus Plus Port
This procedure has been created with Unity Pro v12 software. It will cover the configuration and setup for the MBP_MSTR function block performing an explicit read operation from a node on a Modbus Plus network through the native Modbus Plus port of a Quantum 140CPU65160 processor.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings