Issue:
Wants to program the drive relays to be assigned to indicate transition between local and remote controls.
Product Line:
ATV630
Environment:
All Serial numbers
Cause:
Need to know if local or remote controls
Resolution:
Yes. First, set the HMI Cmd to Bumpless [Complete setting> Command and Reference> HMI Cmd = bumpless]
then Goto [Complete setting> Input/Output > Relay Configuration]
Set R3 to HMI Cmd (BMP:Control via the Graphic Display Terminal is active).
Wants to program the drive relays to be assigned to indicate transition between local and remote controls.
Product Line:
ATV630
Environment:
All Serial numbers
Cause:
Need to know if local or remote controls
Resolution:
Yes. First, set the HMI Cmd to Bumpless [Complete setting> Command and Reference> HMI Cmd = bumpless]
then Goto [Complete setting> Input/Output > Relay Configuration]
Set R3 to HMI Cmd (BMP:Control via the Graphic Display Terminal is active).
Released for:Schneider Electric Nigeria