Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the cable entry size or cable gland size on Altivars ATV650, ATV950?
Sizes of ATV650, ATV950 drives
S-A1 : 0.75kW to 5.5kW
S-A2 : 7.5kW to 11kW
S-A3 : 15kW to 22kW
S-B : 30kW to 45kW
S-C : 55kW to 75kW

Products size Gland CAP
ATV650   A1 1x ISO20
2x ISO25
ATV650   A2 1x ISO20
2x ISO25
ATV650   A3 1x ISO20
1x ISO32
1x ISO40
ATV650   B   1x ISO20
2x ISO40
ATV650   C   1x ISO20
2x ISO63
ATV950   A1 1x ISO20
2x ISO25
ATV950   A2 1x ISO20
2x ISO25
ATV950   A3 1x ISO20
1x ISO32
1x ISO40
ATV950   B 1x ISO20
2x ISO40
ATV950   C   1x ISO20
2x ISO63