Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is ATV900 braking Resistors?
There are three types of braking resistors for ATV900  VSD as below:

light braking cycle
Braking resistors for light braking cycles for machines with cycles and inertia. The braking
power is limited to 1.5 Tn for 0.8 s every 40 s

Medium braking cycle
Braking resistors for medium braking cycles for machines with high inertia and conveyors.
The braking power is limited to 1.35 Tn for 4 s every 40 s

Severe braking cycle
Braking resistors for severe braking cycles for machines with very high inertia and vertical
movements (hoisting). The braking power is limited to 1.65 Tn for 6 s and Tn for 54 s every
120 s

For further information, kindly check the catalog pages attached.

Schneider Electric Nigeria

Attachment(s)
Braking Resistors.pdf [169.25 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: