How can we help you today?

What is the Conditional rated short circuit current (Inc/I∆c) , For RCCB-ID B type ?

The Conditional rated short circuit current :
25/40 A with FU 80 A gG fuse  ==>  10,000 A
63 A with FU 100 A gG fuse   ==>  10,000 A
80/125 A with FU 125 A gG fuse ==>  10,000 A

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: