Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does BMENOC0301 support hold the last value
Question:
Customer has setup his M580 NOC0301 comm with another PLC's NOC using Ethernet IP.
Comm is working all good, however, on his Local Slave side, he wants to be able to change Input Fallback Mode from Set to Zero to Hold the last value but it appears it is grayed out.
Does BMENOC0301 support hold the last value?


Answer:
No, In its current implementation, Ethernet/IP scanner does not support "hold the last value" as input fallback strategy for EIP Devices.