How can we help you today?

What’s the maximum number of words for data in flow variables in BMENOP0300 module?

Question: What’s the maximum number of words for data in flow variables in BMENOP0300 module?
Answer: 4000 words. The maximum number of input words includes the sum of client and server input words. The maximum number of variables depends on the data types included in the application because the lengths of different data types varies. Module memory contains the most current (real-time) value for data in flow.

Schneider Electric Nigeria