Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to order optional ethernet modules for basic version LMC300/400/600 ?

The order number is VW3E701400000. This includes the Realtime Ethernet Optioncard and the backplane to install the card in the LMC.

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: