Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does 383 on the end of the ATV71 part number indicate?
Issue:
Part number ending in 383

Product Line:
Altivar71

Environment:
ALL

Cause:
Special Firmware Requirement for Altivar 71

Resolution:
This was a special firmware version for use with Permanent Magnet Motors.
Current drives ATV600, ATV900, ATV320, ATV340 all have PM Motor parameters by default.