Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to scale Altivar ATV320 analog input to have precisely 25.0Hz when input AI1=5V?
Issue:
Customer needs to scale analog input to have 5V equal 25Hz speed.

Product line:
Altivar 320, ATV320 Altivar Machine

Environment:
All models

Cause:
n/a

Resolution:
By default, the analog input on the ATV320 follows Low speed to High speed in Inputs/Outputs CFG > Reference Template = Standard

To have the drive follow 25Hz with 5V analog signal, set LSP to 0.0 and HSP to 50Hz. Otherwise 5V cannot refer to 25Hz.
If necessary, adjust AI1 min value, AI1 max value, AI1 range, AI1 Interim points X or Y.

See the extracted pages from the ATV320 programming manual attached

Schneider Electric Nigeria

Attachment(s)
Extracted pages from ATV320_Programming_Manual_EN_NVE41295_02.pdf [67.36 KB]