How can I log in after connection to Powerlogic P3 Web server?
Issue
Users need to know which default credentials allow access to the Powerlogic P3 Web Server.
Product Line
Powerlogic P3
Environment
Powerlogic P3 Web Server
Cause
The device uses role‑based user accounts with factory‑set passwords. If these passwords have not been modified, users must log in using the correct default credentials.
Resolution
Use one of the predefined Powerlogic P3 accounts shown below to log in to the Web Server. These default credentials come from the provided device user account table.
Default login accounts:
- Username: user
Password: 0
Used for reading parameters, measurements, and events.
- Username: operator
Password: 1
Used for performing control actions and modifying protection stage settings.
- Username: conf
Password: 2
Required for commissioning tasks such as CT/VT scaling and for HTTP Web Server access
Released for: Schneider Electric Nigeria